Other Parts Discussed in Thread: TMDSHSECDOCK
Hi Chester,
i am using a 5V 3A USB C type power source, surprisingly when i connect the power source to the docking station it works fine, which concludes the power source is fine. but when i connect the USB power source to USB-C type connector(J12) on the TMDSCNCD263 TMDSCNCD263 control card, that doesn't power up the control card.
Regards
Bikash