Other Parts Discussed in Thread: SEGGER, HALCOGEN
Hi all,
I am attempting to set up a simple hello world project on an RM46 Launchpad (RM46L852PGE) target. I am debugging the board via its 20-pin TI JTAG header, using a Segger J-Link and GDB.
I am able to get to a running Application and am attempting to use the RTI Compare 0 interrupt to implement a basic 1 kHz timebase. However, the moment I enable interrupts it appears the processor jumps to an undefEntry handler which is presently the Halcogen-generated infinite loop. I set a breakpoint on the rtiCompare0Interrupt vector, as well as the rtiNotification that is supposed to be called by that IRQ vector after the RTI Interrupt is acknowledged.
It appears somewhere in the jump from rtiCompare0Interrupt() to rtiNotification() that the CPU never makes it there and instead winds up in the undefEntry... Any ideas on what could be causing this?