Other Parts Discussed in Thread: SYSCONFIG
Hi,
using SysConfig 1.13.0 I try to configure the ADC subsystem using all 5 ADC's. Additionally I want to have single ended and differential input signals converted. However sysconfig does not allow me to mix single-ended and differential inputs for the very same ADCx of the chip.
Q: Is this a limitation of the chip or of system config?
br
Markus
Differential inputs signals are shown in blue. What I am asking is for ADC3 and ADC4 in this context. If it is not possible, then I would need to reasign the signals to make sure single ended inputs and differential inputs are well separated on a per ADC base ... Is this so?