Hi Team,
Could you please share the correct connections for JTAG 10 pin interface? Below is customer drawing and they are looking for feedback. Thanks! Reed
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Could you please share the correct connections for JTAG 10 pin interface? Below is customer drawing and they are looking for feedback. Thanks! Reed
For 10-pin JTAG header, the pin 10 is for nRESET (system reset). Pin 10 can not be used for nTRST.
The 10-pin Arm JTAG connector doesn't include the nTRST signal. Without this signal, the TMS570 JTAG TAP controller will be held in reset by the internal and external pull-down that is recommended for the TMS570 TRSTn pin. This will make it impossible to communicate with TMS570LSx via JTAG.
Thank you very much, QJ. Could you share any reference schematic that the customer could use for reference?
Hi Reedkacz,
Please refer to my note about the JTAG connection:
https://software-dl.ti.com/hercules/hercules_docs/latest/hercules/FAQ/FAQ.html#jtag-connection
You can also refer to the launchpad schematics about the JTAG signals connections. The launchpad is small and the JTAG signal trace is very short, so we don't add series termination resistors on JTAG signals.
QJ - perfect thanks. The customer has updated and is shown below. Could you please take a look to make sure it is OK? Thanks!
Hi ReedKacz,
1. The RTCK is not a standard JTAG signal, so leaving it NC is OK.
2. If nTRST is not connected to emulator, the nTRST should be pulled HIGH on your target PCB board. If nTRST is connected to debugger or emulator which has an internal pull-up on nTRST signal, a pull-down is added to nTRST on target PCB board.