This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: Clarification on EMIF_CLK max frequency

Part Number: TMS570LS3137

Hello,

I write to have a confirmation on the spec of the signal EMIF_CLK:

The example at "17.2.5.6.1 Determining the Appropriate Value for the RR Field" and the whole "17.4 Example Configuration" chapters of the TRM set f(emif_clk) to 100MHz.

In the TMS570LS3137 datasheet, the "Table 6-27. EMIF Asynchronous Memory Timing Requirements" sets the minimum EMIF clock period to 11ns (i.e. up to 90.9MHz), but in the "Table 6-30. EMIF Synchronous Memory Switching Characteristics" the minimum EMIF_CLK cycle time is 20ns (i.e. a max frequency of 50MHz).

Can you please clarify which is the max EMIF_CLK to use for both SDRAM and async devices?

Thanks in advance,
Federico.