I compiled one of the TivaWare_C_Series-2.2.0.295 board examples for the EK-TM4C1294XL board. The example is: enet_tcpecho_server. It works fine as a server but when I try to add code to use TIMER0 I am not able to use the TivaWare example code found in the timers folder. The enet_tcp_server application works fine when I lower the priority of the TIMER0 interrupt to 0xE0 but then I never hit a breakpoint the TIMER0 ISR. I am configuring TIMER0 to run at 400Hz.
Is there anything special about using lwIP and TIMER0?
Thanks for all your help.
Jorge