Other Parts Discussed in Thread: TMS570LS3137, LM4132, HALCOGEN
HI TI team,
We are planning to operate (ON/OFF) LM4132-2.5V Reference IC by using GPIO port B of TMS570LS3137.
LM4132 input voltage is 5V and EN pin is pulled up with VIN for 2uA asper datasheet specification. So if I left floating for EN pin and measure the voltage it will be 5V.
TMS570 GPIO port B has the option of open drain output, and it can be configured using HalcoGen. So no needs to use external transistor.
We are planning to use Open drain configure to pull down EN pin of LM4132 to turn ON and OFF the Reference voltage.
TMS570 recommended Maximum voltage applied to GPIO is 3.3V.. My Query is that if I connect as described above it will create any issue with Microcontroller.
Please kindly share the feedback.
Thanks and Regards,
Venugopal