1. In the 8.6 sdk, only profinet_ device\icss_ Fwal, there is no profinet demo provided. May I know where to obtain the profinet demo project or when it will be released?
2.Do PN protocol stacks require external DDR?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. In the 8.6 sdk, only profinet_ device\icss_ Fwal, there is no profinet demo provided. May I know where to obtain the profinet demo project or when it will be released?
2.Do PN protocol stacks require external DDR?
Hi Cheng Zhijun
In the 8.6 sdk, only profinet_ device\icss_ Fwal, there is no profinet demo provided. May I know where to obtain the profinet demo project or when it will be released?
Profinet demo will not be part of SDK 8.6. It will released as a patch on top of 8.6. The schedule for the same is not finalized yet. I will notify here once we have it out, or else you can check on ti.com page
Do PN protocol stacks require external DDR?
Yes the current memory foot print of PN stack is more than 2MB, so it will require DDR.
Could you please tell me what is your use case, we also have 3rd part like TMG who enable PN stack under 2MB which will not need DDR.
We have plans to optimize the PN stack, timeline for same in 2024
Could you please tell me what is your use case,
Using AM2434 as a gateway for PN or EIP or ECAT.
we also have 3rd part like TMG who enable PN stack under 2MB which will not need DDR.
The previous SDK used Kunbus's PN protocol stack, but it was no API to obtain user configuration information on PORTAL. Could you provide the TMG‘s PN protocol stack DEMO for AM2434 .Is it free, and has it passd the PN testing and certification?
Using AM2434 as a gateway for PN or EIP or ECAT.
Could you please explain more about the gateway, is it IO-Link gateway?
You can refer this for ECAT gateway:
The previous SDK used Kunbus's PN protocol stack, but it was no API to obtain user configuration information on PORTAL. Could you provide the TMG‘s PN protocol stack DEMO for AM2434 .Is it free, and has it passd the PN testing and certification?
Yes they have already passed the certification. For demo you need to contact TMG, and they will be charging a fee.
Could you please explain more about the gateway?
Such as translate ECAT or EIP or PN protocol communication to modbus communication .
Got it. Please take a look at this : software-dl.ti.com/.../INDUSTRIAL_COMMS_TI_STACK.html
Profinet demo will not be part of SDK 8.6. It will released as a patch on top of 8.6. The schedule for the same is not finalized yet. I will notify here once we have it out, or else you can check on ti.com page
Could you give me an estimated release time for the PN demo?
Does the new PN DEMO need to be run on the new AM2434 development board?
Could you give me an estimated release time for the PN demo?
An estimate plan is to get it out by end of this month.
Does the new PN DEMO need to be run on the new AM2434 development board?
This demo needs to be run on am243x gp evm, as the memory requirement is for more than 2MB.
An estimate plan is to get it out by end of this month.
Do you have a definite plan when to release the PN demo?
Hi Cheng,
Apologies for delay in response.
The licensing is not yet finalized. I apologize for the inconvenience caused due to logistical delay on our side.
Given the nature of problem, it is quite difficult for us to communicate the exact dates.
Best projection we have for the dates is SDK 9.0 release in End of August 2023