This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1303: OpAmps, Peak-to-peak input noise voltage

Part Number: MSPM0L1303


We are working on designing a sensor solution using the MSPM0L130x. The plan is to utilize the internal OpAmps for the analog circuit. However, we have been unable to locate aparameters in the electrical characteristics of the chip. Could you please provide us with the Vn (pp): Peak-to-peak input noise voltage from 0 to 1Hz and from 0 to 10Hz (in uV peak-peak).

This parameter is different from En, which represents the input voltage noise density in nV/√Hz. En describes white noise, whereas Vn (pp) describes 1/f noise. 

I specifically need the Vn (pp) value because we intend to use the internal Opamp in a circuit where Vn (pp) is the dominant source of noise. They are small signals with long time constants, resembling a DC-like signal.

Thank you.