This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About I2C write for ISET setup and some config. parameter by LED171596AWVM

Part Number: EK-TM4C123GXL


Hi Team,

Here're some issues from the customer may need your help:

I need to control some LEDs (duration 10-50ms; Frequency 10-50Hz; Current 10-600uA; ) by using LED171596AWVM with TM4C123GXL. I already maximized the maxBri and the MasterBri with 0x1ff. So, the PWM should be 100%. The current output should only rely on the current value itself. However, I have some issue regarding ISET setup and some config. parameter.

1) I know how to set them but I don't know how parameter of the LED Driver, PWM and Sloper config, is reasonable to my project? (as fig,1)?

2) I can see the log in EVM software and I can select them (e.g. 10mA, 12.5, ..., 60mA) (as fig.2). But I don't know how to I2C write this ISET to initial peak current with a program?

--

Thanks & Regards

Yale