This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM243X: MCRC

Part Number: MCU-PLUS-SDK-AM243X

Hello IT-Support,

in chapter "12.6.3.1.1 MCRC Features" in the documentation "sprum2g.pdf" says there are 3 Modi to use.

- Auto Mode, Semi-CPU, Full-CPU

But in chapter "12.6.3.1.2 MCRC Not Supported Features" says that there is no DMA support and Auto - Mode support.

-> Do i understand right ? Only Full-CPU Mode works yet ?

In "mcu_plus_sdk_am243x_08_06_00_43" there are examples for Auto Mode, Semi CPU and Full CPU. But only Full CPU example works.

In "mcu_plus_sdk_am243x_09_00_00_35" there is only Full CPU example.

When will the other Modi be implemented?

Is there a significant impact on memory bandwidth or bus load in the different Modis?

Is there a impact to use the mcrc parallel with all cores with freeRTOS?