This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: No syscfg file for examples projects using CC1310 Launchpad

Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310, SYSCONFIG

Greetings

I have been struggling to integrate a syscfg file into code composer studio. From tutorials and TI training as well, a syscfg file should be generated with an example from the SDK. I'm able to see this when I open an example with a CC1352-Launchpad, where I have opened examples and there was a syscfg file.

Is there a clear guide available on generating an integrating an syscfg into a project for the CC1310, or is there a reason why the SDK examples do not generate the syscfg file?

Any help would be appreciated.