This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3107-Q1: I/O pin protection

Part Number: MSPM0G3107-Q1


hello,

i have one question about the I/O pin 

As shown in the figure below, Mcu's I/O port is equipped with a clamp diode

1)I want to know if I/O will be damaged when there is forward overvoltage and reverse overvoltage at the I/O port? 

If it will cause I/O damage, Is damage caused by overcurrent? Overcurrent caused by high voltage?

2)another question: When I apply  an AD port, Should I connect R2, resistors in series in the AD acquisition circuit?

please help check this follow AD acquisition circuit ,and the VIN input Power is 13.5V, Is there a problem with the circuit?My software sampling cycle is every 2ms

How do I set the values of R2 and C2 value,please help explain in details.

thank you

best regards 

  • The absolute max voltage on an IO pin is Vdd+0.3 V, or -0.3 V. Note that when Vdd is off (Vdd = 0) anything above 0.3 V is not allowed - and in fact can power the chip. (As I learned the hard way). Absolute Max ratings follow the pottery barn rule, if you exceed it, you bought it.

    The clamp diodes can sustain *some* level of current, but it is wise not to depend on that, and avoid it completely.