This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: Can we have a quarter-cycle sine taper in a digital pot to use in u-power u-controller electric guitar circuits?

Part Number: MSP432E401Y

Tool/software:

Please have a look at Fig. 17 in U.S. Patent 10,380,986; Fig. 16 in 10,810,986; Figs. 10, 11 & 21 in 11,087,731; Fig. 53 in 12,020,674; and Figs. 18, 26, 30 & 31 in US2023/0013236 A1.  I've been designing these circuits in mind for TI micro-power op-amps and TSP430 and 432 micro-controllers, to run for more than 100 hours on AA batteries.  I can see a large place for a micro-power digital pot with a quarter-cycle sine taper, to use in the linear mixing of humbucking pair string signals.  I have two more patents in mind.  

But I'm limited to filing and prosecuting patents.  I don't have the resources for anything else.  Plus age and medications have removed my software skills.  I need partners.  

Any bites?