The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM243X: Hardware question: custom board problem communication between am243x and m3.

Part Number: MCU-PLUS-SDK-AM243X

Tool/software:

Hi, 

After building a customized board, the internal communication between the AM243x and the M3 is not functioning, and the board gets stuck at the Sciclient indefinitely. We built a few boards, and while most of them work fine, one is experiencing this issue. We tried switching a few CPUs on the faulty board, but the problem persists.

If the R5F sends a corrupted message to the M4, what is the likelihood of an issue with a peripheral pin (e.g., a pin that should be low is accidentally set high)?

Thanks

  • Hello Jun Tu,

    After building a customized board, the internal communication between the AM243x and the M3 is not functioning, and the board gets stuck at the Sciclient indefinitely.

    Can you please confirm for which operation R5F/M4F core is not getting any response from M3 core ?

    Since all device management and security operations handled by DMSC (M3) Core  like, reset, clock, interrupts and security functionality etc. through SCI client calls.

    So, definitely R5F / M4F core should send the SCI client request to get a response from M3 Core.

    Tell me the SCI client API with what parameters are sending when M3 is not responding.

    Regards,

    Anil.

  • Hi, Swargam, we can be sure, it is a hardware problem.  after production, 40% of boards has this problem. 

    we are trying to run sciclient_ccs_init.release.out, and reach hello world.    but with 50% of these defect boards, it can't reach hello world. 

    Then, I build sciclient_ccs_init.debug.out. For defect board,  it will stuck at this message. (For good board, it won't have this problem.) 

    but what could be the pin affect this behavior, there are too much pins to compare. do you have a list?  there are too many pins to compare, so far we didn't find the difference.  So if there are list of possible pininput corrupt the communication.





    So two reason. 1. data send to dmsc is corrupted.   (looks like the issue) 2. we don't receive the ack whatever back.

    which list of pins will affect bus between m3 and r5f?

  • so eventually, the defect board, will stuck at sciclient_waitformessage forever. 

    by using debug, we found, CUR_CNT, is already not right when sent the message. 

  • but what could be the pin affect this behavior, there are too much pins to compare. do you have a list?  there are too many pins to compare, so far we didn't find the difference.  So if there are list of possible pininput corrupt the communication.

    Hello Jun,

    You are talking about which pins ?

    I really don't understand the above point.

    Typically to configure GPIO pins we never  calls SCI client .

    The sysfw has a bin file which will include in SBL and SBL will initialize SYSFW.

    This is how we are following the method to initialize SYSFW on AM64X/AM243X devices .

    Regards,

    Anil.

  • Hi, Swargam:

    We are encountering a hardware issue with our customized board. It seems that there might be a problem with either a bad pull-up or a bad ground on some pin, or possibly a mistake in the design or assembly. About 50% of the boards are functioning correctly, but the other half are experiencing issues.

    Due to the large number of pins, it is very challenging to pinpoint which specific pin might be causing the problem or generating noise.

    From a software perspective, the issue manifests as a failure during the sciclient wait. This indicates that the communication between the R5F and M3 processors is breaking down.

    Could you help us understand how to approach diagnosing this issue, both from a hardware and software standpoint, to identify the problematic pin(s) and resolve the communication failure?


    Thanks.


    By the way, Software gpio init has nothing to do with that, I completely agreed with you. Typically to configure GPIO pins we never  calls SCI client ..  It is definitely a hardware problem. it might be some noise added into internal bus between r5f and m3.

    or can you point me a internal hardware schematics for r5f and m3, so we can take a look which pin might affect bus communication between r5f and m3. Thanks

  • Hello Jun,

    You can just see the SBL logs,  based on this information we can confirm that the board is Resetting frequently.

    Or try to connect to CCS and see every time the debuggers shows Reset is initiated or not.

    Then monitor the power supply pins of SOC if the GND is floating and not connected properly to SOC this is also a problem.

    And, monitor all Reset Pin status and see the these pins creates an issue or not.

    Actually, if you are not using any pins, then those pins definitely will not create any problems.

    So, we need to monitor all reset pins as the first step.

    Regards,

    Anil.

  • Hi, Anil, Thanks, after we focues on the reset pin that you just mentioned, we found the problem and now, it run succesfully. 

    Again, many thanks for your support.

  • Hello Jun,

    Good to hear that you have solved the issue.

    I am closing this thread now and open new threads for new queries.

    Regards,

    Anil.