Part Number: TM4C123GH6PM
Tool/software:
Hello,
I have reviewed datasheet section on power consumption, but I could not find relevant info. I would like to power the tm4c123gh6pm via a low-noise, high pssr LDO.
Usually I use a TPS73633 which is 0.4A.
What is the lowest current that I can get away with? Will a 0.25A or a 0.3A LDO be ok?
The reason I would like to do this is to feed my crystals with low noise input, and I could probably use different power for the crystals, but before that I want to see if i can power the whole thing with a low noise LDO.
Best Regards,
Can