Other Parts Discussed in Thread: AM2634, AM2434
Tool/software:
Hi all
I'm testing CPSW peripheral on LP_AM2634 board using MCU_SDK_10_00_00_31.
I'm able to open the driver correctly and TX/RX frame from/to a Windows PC.
But I have some question open.
1) How can I get the speed of the link and the duplexity from the driver.? I expect a speed of 100Mb but the routine I wrote give me only 2Mb
2) What is the correct way to configure CPSW to have a PHY connection towards the eaternal world on one port and a MAC connections internally to the same demo board using SysCfg? Do this configuration supported by AM2434 and by SysCfg?
3) An architecture similar to the following is feasible? If yes I need two R5F core so do I need a system project?
PHY0<-->CPSW0<-->MAC0 <---> MAC1<-->CPSW1<--> PHY1
| |
R5F00 R5F10
Thanks in advanced
Best regards
M