This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1306: Unable to add "Configuration NVM" to sysconfig on MSPM0L1306-WQFN-16(RTR)

Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG,

Tool/software:

I'm trying to add "Configuration NVM" to sysconfig on an existing MSPM0L1306 WQDN-16(RTR)  project. However, the UI warns me of exceptions when I click the Add button. In order to discard any error on my current sysconfig or project, I've generated a new fresh empty project for my device but, unfortunately, the same error message is shown as soon as I try to add here the "Configuration NVM" option in sysconfig. 

These are the steps I follow to replicate the error:

  • Create a new empty project for MSPM0L1306 using "No RTOS" and "CCS - TI Arm Clang". This will create a project targeting MSPM0L1306-VQFN-32(RHB)

  • Open empty.syscfg and change the device package to WQFN-16(RTR)

  • Try adding Configuration NVM

  • An error message is shown

Some other things I've tried:

  1. If I switch back to package VFQN-32 (RHB), I can add "configuration NVM" without any problem.
  2. If I add "configuration NVM" when package is VQFN-32 (RHB), switching once more to WQFN-16(RTR) results in the same error.

I'm working with Code Composer version 20.2.0.12, Sysconfig  version 1.24.0 and MSPM0 SDK  version 2.5.0.05.