This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error 135 while flashing TMS570LS3135 with nowFlash v3.41

Other Parts Discussed in Thread: TMS570LS3135, TMS570LS2125, TMS570LS3137, RM48L950

Hi!

I've some problems flashing a TMS570LS3135 device with nowFlash v3.41. I use a Spectrum Digital XDS510USB debugger and get the following error message:

A quick check of the nowFlash.cfg file shows, that the device ID 0x802AAD05 identifies the configuration sections for a TMS570LS3137, a TMS570LS2125 and a RM48L950. I am not sure which of these sections is applied but no configuration sets the right cpu frequency for this device which I've overwritten from the nowFlash GUI to be 160MHz:

I'he also checked that "Scan Chain 0" is disabled and Big Endian is enforced in the configuration of the XDS510USB. I also tried to use the -w option with values from 1 to 10 with no success.

Could someone give me a hint, whats going wrong here?

Thanks in advance,

Christoph