Part Number: F28M36P63C2
Other Parts Discussed in Thread: UNIFLASH, C2000WARE,
Hi,
I'm using my F28M36P6 card via a docking station. However, I can't load the code to the card via JTAG. When I connect to the card via USB (XDS100 v2), there are no problems; I can connect to both CPUs (M3 and C28) and upload code to flash. However, when I try to load code using the JTAG pins on the docking station with an XDS220, I can only connect to the M3 chip, not the C28. The error code I receive is as follows:
"Error connecting to the target: (Error -1015 @ 0x0) Device is not responding to the request. Device may be locked, or the debug probe connection may be unreliable. Unlock the device if possible (e.g., use wait in reset mode and power-cycle the board). If the error persists, confirm the configuration and/or try more reliable JTAG settings (e.g., lower TCLK). (Emulation package 20.4.0.3835)"
(I'm paying attention to A:SW1 pin configuration for JTAG connection, but i think this error is not about that)
Then, I tried connecting via UniFLASH and viewing the data packets in memory. When I connected with the XDS100 v2, I could connect to both processors and view their memory. However, I couldn't connect to the C28x via JTAG (XDS2xx) and received the same error code.
Then I tried this: I connected to the board with the XDS100 v2 and unlocked the CSM PSWDs/KEYs option in the C28x settings. After that, I erased the flash memory. I tried connecting again via JTAG, but it still didn't work.
By the way, when I click the test connection button in the .ccxml file in CCS, both CPUs connect successfully. However, when I try to upload a program to the C28x, I get the same error again.
Additionally, I reduced the connection settings from 10.0 MHz to 50 KHz, but I still get the same error.
To sum up, i dont think that C28x is broken because i can connect and load program via XDS100v2 (Internal emulator on the board). But, i cannot connect and load program via JTAG (XDS220 ISO, External emulator) and got the error above.
Could you please help?
Thank you,
Sincerely