This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-IOBKOUT - GPIO Breakout BoosterPack without Voltage Follower Op Amps

Are there any plans to make a BOOSTXL-IOBKOUT - GPIO Breakout BoosterPack without the Voltage Follower Op Amps?  In my opinion making the BOOSTXL-IOBKOUT - GPIO Breakout BoosterPack with the Voltage Follower Op Amps was a poor decision.  I just spent the weekend unsoldering the Op Amps and adding jumpers on 3 of the boards so I could use the BOOSTXL-IOBKOUTs with a BOOSTXL-SENSHUB and other applications that need those pins for non-analog I/O.  The Op Amps could have been easily added externally if required.  Also why only one VBUS pin and so many 3.3V?