This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TIDM-TM4C129XNFC: Issue building NFC sample code for EK-TM4C1294XL with RTOS 2.16

Part Number: TIDM-TM4C129XNFC
Other Parts Discussed in Thread: CC31XXEMUBOOST, CC3100BOOST, EK-TM4C1294XL, UNIFLASH, CC3100

Tool/software: TI-RTOS

Hi,

I need to read ISO14443A/B Type 4 NFC cards, so I’m using: 
To support this software I have the following hardware, which includes two options for NFC (7970A & RF430).
My questions are:

  1. Is the CC31XXEMUBOOST only needed to flash / copy files to the CC3100BOOST and therefore should NOT be connected with running the NFC software?
  2. Page 17 of tiduag2a.pdf specifically asks for RTOS 2.14. Is RTOS 2.16 ok to use instead?
  3. What Target Config "Tiva C" card should I be using with a EK-TM4C1294XL? Is the Tiva TM4C129NCPDT ok since the EK-TM4C1294XL is not listed?
  4. I get the errors shown in the screenshot when trying to build the NFC sample code, what should I do to get it working?
Thanks in advance for your help!
Cheers,
Tim