This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129CNCZAD: Crystal selection for custom TM4C129x board

Part Number: TM4C129CNCZAD
Other Parts Discussed in Thread: CC1310

We have a 24 MHz crystal that we use with the CC1310, and we would like to use it with the TM4C129x processor we have selected in order to keep our BOM easier to maintain.  After reading through the Clocks section of the datasheet (Section 29.9.5), I still have two main questions:

1. Will the Epson TSX-3225 24.0000MF15X-AC6 (with a load capacitance of 9pF) work for this chip if I use 10pF load capacitors?

2. Will using a 24 MHz crystal cause any weird clock issues with the UART, CAN, or USB peripherals using MOSC as their clock source?

I will admit, this is my first custom board design with the Tiva series chips, and I am transitioning from a different architecture to the Texas Instruments ARM architecture.  However, I did use the math laid out in Section 29.9.5 before posting here.

Thanks in advance.