Other Parts Discussed in Thread: TM4C123GH6PZ,
Dear,
There is a usb_stick_update example in DK-TM4C123G. Since it uses TM4C123GH6PG (144 Pin), the USB pin in Example is PL6/PL7 (USB0DP/USB0DM). However, the MCU I used is TM4C123GH6PZ (100 Pin). The USB pin is PJ0/PJ1. I tried to modify the corresponding PL6 and PL7 in usb_stick_update to PJ0 and PJ1. However, the program cannot perform USB firmware update. Does the usb_stick_update in DK-TM4C123G have a chance to be modified? Executed on TM4C123GH6PZ?