I would like to write some data to flash bank 7 using IAR and a J-Link flash loader. Is it possible to place const variables in a sector within flash bank 7 that are initialized with non zero values? Can the flash loader write the initial values to the corresponding flash bank 7 memory locations or is this only possible using the TI F021 Flash API? The J-Link flash loader can write directly to bank 0 and bank 1, so is there any limitation preventing the loader from writing directly to bank 7?
In the scenario above i am not using EEPROM emulation, but simply want to write data to flash bank 7 using the IAR tools.
Thanks,