This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1230E6PM: USB-to-JTAG

Part Number: TM4C1230E6PM
Other Parts Discussed in Thread: CODECOMPOSER

Is it possible to get the source code for the USB-to-JTAG debug tool (part of the TIVA launchpad).  We are using this device on the new active-control-system (ACS) part of the W.M. Keck Observatory to handle the tip-and-tilt of the 36 mirror segments.  There are two TM4C1230 per segment (one for the USB-to-JTAG, the other for the capacitive sensor monitors) the system monitors and reports the position of each of the six sides of each mirror segment with respect to its neighbors (with a precision of +/- 3nm).  In the prototypes we depopulated the USB-to-JTAG device (from the TIVA Launchpad) and placed it on our PWB so we could use CodeComposer for debugging the design and downloading the code to the other TIVA device on the board.  In the final system we would like to program this device with the USB-to-JTAG code.  Please let us know if it is possible to get the source-code.  Thank you, John