Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/HERCULES-DSPLIB: Pre-Compiled HERCULES-DSPLIB for Linux (in the format of .a)

Part Number: HERCULES-DSPLIB

Tool/software: TI C/C++ Compiler

Hello all ,

I have found HERCULES-DSPLIB CMSIS library provided by  TI which has  source code as well as  pre-compiled libraries but these library are in .lib format which is basically supported for Windows .

Can anyone help me giving information about  HERCULES-DSP precompiled library for linux platform (i.e in the format of .a) also dependencies of same library ,If I want run sample application on linux linking these libraries .

Regards ,

Manish