Part Number: TIDM-NFC-SDM
Other Parts Discussed in Thread: TRF7970A
Hey hi ,
I am working with NFC technology and currently using most commonly used MFRC522 IC and tags we are using is MIFARE Classic 1K.
Now we have to switch to other NFC Tag Reader-Writer IC for better performance in case of:
-Tag Detection Range
-Power Consumption
In initial searching I found TRF7970A and TIDM-NFC-SDM .
And moreover we have to use anyhow MIFARE Classic 1K Tags only , so query is that can we use the above IC/EVM for reading and writing the MIFARE Classic 1K Tags , because what I know is the "Authentication" used in such type of tags , so is the authentication layer is included in TRF7970A ?
If not so , please suggest me the proper IC so that it can be directly used for reading-writing the MIFARE Classic 1K tags with proper documentation or sample source code, so that it can take less time for product development.
Regards,
Vaibhav P