Part Number: TMS320F28386S
Other Parts Discussed in Thread: C2000WARE
Greetings,
I am porting code from a 379D project to the 386S, and have told the linker to produce a TI-TXT output file. When I examine that file, I see the sections I expect to see. But I also see another section I cannot explain. It contains text (maybe Unicode?) which is not part of the code. It also contains a class name which is part of the source code, but should not be in the output of the build process. It is all in the .const section which is currently mapped to flash. A snippet of the TI-TXT file is below. What is causing the extra information? Is there a setting I need to use to remove it from the final output?
Thank you,
Ed
@<my address>
4E 00 31 00 30 00 5F 00 5F 00 63 00 78 00 78 00
61 00 62 00 69 00 76 00 31 00 32 00 33 00 5F 00
5F 00 66 00 75 00 6E 00 64 00 61 00 6D 00 65 00
6E 00 74 00 61 00 6C 00 5F 00 74 00 79 00 70 00