This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Controlling ACTIVE and REACTIVE power in the C2000 Solar micro inverter Kit



Hello Manish, 

I am using the New solar micro inverter kit and I have done the full set-up and  its working perfectly via the GUI, great piece of equipment

I want to modify the code so I can control real power flow and the secondly to control reactive power flow through the micro inverter board.

Please can you advise me on the area of the code where changes is needed so that key parameters such as power angle and voltage magnitude can be altered:

PS: if there is another better way to do this I will appreciate it- 

regards

Solomon