Hi
There are two definitions in user.c file,for oneOverDcBus para.
pUserParams->oneOverDcBus_min_invV = (float32_t)1.0 / (float32_t)400.0;
pUserParams->oneOverDcBus_max_invV = (float32_t)1.0 / (float32_t)10.0;
Does it matter in motor control situation?
If I want to use in more than 400V situation, should I change the pUserParams->oneOverDcBus_min_invV value?
Regards
Arrow