Other Parts Discussed in Thread: DRV8301, BOOSTXL-DRV8301,
Hello, I am developing our motor control hardware using the TMS320F28069M and a BoostXL-DRV8301 boost board. I see that from the DRV8301 datasheet that if 3.3V is being used by the BoostXL that one should disconnect the 3.3V jumpers JP1 and JP2 on the TMS320F28069M board (which is derived from the USB and limited in current).
Is it possible to supply an external 3.3V to both the F28069M and DRV8301 board or is the 3.3V generated on the DRV8301 IC?
Regards, James