Part Number: TMS320F28388D
Other Parts Discussed in Thread: TMDSCNCD28388D
Trouble Reading Register PC:
(Error -1156 @ 0x0)
Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device.
(Emulation package 9.2.0.00002)
When I power on the board, I plug in the emulator first, and then power on. Use CCS10.0 to download the program to RAM, it can be downloaded normally. But when you choose to download to FLASH, an error will be reported, as shown above.
The power chip used by my circuit board is: TPS62420DRCR
The output of this chip has two channels. The current can reach 1000ma (1.2V) and one can reach 600ma (3.3V).
For the chip, there will be a certain amount of pressure on the load (I want to ask if this is the reason for the above error.) (Error -1156 @ 0x0)
I considered this situation, so I removed a lot of components on the board (LED light, DC-DC module), touched the power chip for a while, and found that the temperature was normal. When soldering the small LED lights and DC-DC modules that were removed before, the power chip will be very hot.
After removing the LED light and DC-DC module, power on the board and download the program to FLASH, the above error will still occur. (Error -1156 @ 0x0)
Download to RAM, it can still be downloaded normally.
Here to ask
thank!
vince