Hello support team,
F28002x has 16bit Word memory map, e.g. Sector 0, 4K x 16, 0x0008 0000 to 0x0008 0FFF. When I go to a addess, I get a 16bit Word.
- Can I also acces a byte using address? Does high byte at addess 0x80000 have its eigen address?
- When I generate a Intel HEX file with "--memwidth=8 --diag_wrap=off --intel", the adress is doubled. the first adress is 0x100000 instead of 0x80000. With "--memwidth=16 --diag_wrap=off --intel" I have correct address but 2 files *.hex and *.i01 for high byte. Can I flash the HEX file like this topic in both cases (memwidth=8 and memwidth=16)?
In case of memwidth=16, should I flash 2 files or the SW can automatically join both *.hex and *.i01 files?
Regards,
Nguyen