Hi,
when I press the debug buttion (green bug button) in CCS 6(while the compiler version is V5.2.8), there seems that boot28.inc can not be found, the message shows"Can't find a source file at "/sim/sds12/scratch/jnash_rtsbuild_dflcmp2510.dal.design.ti.com_24979_linux/ank_rts/boot28.inc"
Locate the file or edit the source lookup path to include its location."
I actually installed several compiler version include "V5.2.8, V5.210,V6.2.0, V15.12.3,V16.9.6 ". When I try to search boot28.inc file in my computer, it can only be found in V15.12.3. Since my project is an old project , and if I use the compiler V15.12.3, the project can not pass the compilation. Among the compiler version above, only V5.2.8 can pass compilation, which is also usded in the old project.
And once the problem shows, there is a hint which requires you to to locate the file boot28.inc. For now, I can only locate the boot28.inc file in the compiler‘ library, the version of which is V15.12.3.
Since the compiler I used in V5.2.8, however I should use the library file (boot28.inc ) in V15.12.3. Currently, the message 'Can't find a source file at "/sim/sds12/scratch/jnash_rtsbuild_dflcmp2510.dal.design.ti.com_24979_linux/ank_rts/boot28.inc' will not show again, but the problem now seems that the project does not jump to main normally and stop there.
My quesion is that "why compiler V5.2.8" has to use the libraty file in V15.12.3. How the old project work while the the new compiler hasn't been developped. Is there any problem I use the library file in the new compiler while i use old comipler to compile the whole project.
Thanks a lot for your help
Lookforware someone could reply.
Chao