Other Parts Discussed in Thread: UNIFLASH
Hello support team,
I have 2 SW (2 hex files):
- SW1: custom bootloader with entry point 0x80000
- SW2: application with entry point 0x84000 (or 0x83000)
I want the boot sequence as following
- CPU Boot Start. Flash boot
- Branch to Flash Entry Point of SW1 (custom bootloader)
- custom bootloader do something
- SW1 jumps to Flash Entry Point of SW2 (application)
My question is:
How can I modify the cmd file of SW2 so that when I both hex files at a same time with Uniflash, the device boot will branch to entry point of SW1 in step 2 (not entry point of SW2)?
Regards
Quy