Hello E2E,
Our customer is using the LAUNCHXL-F28027F with BOOSTXRL DRV8305EVM to run a BLDC motor and they get an error in using CCS version 10.
Need your help with the workaround on the error. Thank you.
Regards,
Carlo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello E2E,
Our customer is using the LAUNCHXL-F28027F with BOOSTXRL DRV8305EVM to run a BLDC motor and they get an error in using CCS version 10.
Need your help with the workaround on the error. Thank you.
Regards,
Carlo
Hi Carlo,
Looks like one of the sections is too big and the linker is unable to fit it in the available memory block.
Please update the linker command file to use more memory blocks for that section.
Eg: .text : >> RAM1 | RAM2...
You can check the .map file to check the sizes of the sections and the available memories in the RAM and Flash blocks
Regards,
Veena