This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386D: SPI: Only start transmission after FIFO loading

Part Number: TMS320F28386D

Hello,

I have a particular use case where I want to be sure the FIFO is fully loaded before I start the exchange with the slave (CPU is MASTER).

The reason is, as the peripheral frame is shared with the DMA, I have to ensure the words are in the FIFO to be sure I respect the protocol awaited by that salve.

Is there a way to achieve that ?

I have the feeling, from the registers fields descriptions, that this is not something feasible.

Best regards,

Clément