The F28035 requires GPIO34 == 1 and GPIO37 == 1 in order to get into OTP_Key Boot Mode GetMode selections. However, on the TMDSDOCK28035, GPIO37 is TDO which is used for the JTAG. How does one wire up the DOCK in order to get into the OTP_Key Boot Mode GetMode CAN bootloader while developing and debugging? Do I need to put a pull up resistor on GPIO37/TDO when in OTP mode with no emulator and then pull it off when I want to use the emulator again? (Add a switch the the DOCK so pullup closed/open?)