Part Number: DRV8312-69M-KIT
I imported proj4a, clean, build the project. It generated binaries in CCS . Then I debug it and connect to the target configurations and load the program to the control card.
After that I copy the proj4a. out and target.ccmxl file to the ti/GUI composer /web apps.rename it as appProgram.out, appConfig.ccmxl file. Try to open the instaspin FOC application .just like default software it initializes the target, but coming to the application side the KIT didnt identified and all the automatic updating value icons shows cross mark.
How should resolve this problem and to run the motor .