Other Parts Discussed in Thread: C2000WARE
Hi champs,
Do we have any GUI which supports the ROM-based bootloader via SCI or CAN?
Regards,
Kien Nguyen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi champs,
Do we have any GUI which supports the ROM-based bootloader via SCI or CAN?
Regards,
Kien Nguyen
Kien,
We use a windows based application called serial flash programmer, which is available in C2000Ware. It isn't a GUI.
It helps you download an image from the host (PC) to the target (C2000 MCU). The ROM-based bootloader (SCI) can be used to download a bootloader (called a SCI Flash Kernel) to RAM, and then this bootloader will run in RAM to download an Application to Flash.
For details, please refer to sprabv4
Thanks,
Sira