Part Number: TMDSCNCD28069
Other Parts Discussed in Thread: C2000WARE
Hi!,
I am using Piccolo F28069 (TMDSCNCD28069 R1.1) for Motor control Project with the help of a speedgoat machine . early its working fine, but now when i try to flash the program , it show an error like below screenshot.

Error :C28xx: Failed CPU Reset: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.2.0.00002)
.;.When i try to find the solution for the error , i got a Ti forum with same error but different control card .(link :CCS/TMS320F28035: Troubleshooting Procedure for error"C28xx: Failed CPU Reset: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 6.0.576.0)" - C2000 microcontrollers forum - C2000︎ microcontrollers - TI E2E support forums )
So i follow the steps . what i got from that ,when the Brett Larimore ask to check the XRSn pin .So when i check it I got 0V rather than 3.3V ,now i am stuck here .what should i do next..is there any further troubleshooting i can carry out to resolve this issue of TI control card?