Other Parts Discussed in Thread: C2000WARE
When a new F28035 requires code, you can pull up GPIO37 and pull down GPIO34 to configure boot mode to SCI. So a new F28035 without code will sit and wait until a hex file is loaded via SCI. Once code is loaded, the resistors haven't changed and would effect all future power on cycles. What do designers typically do for these 2 pins because I believe they would be sampled by the bootloader before you could configure them as outputs. Do designers typically use headers and jumpers for the first code load so that on the next power cycle removing the jumpers removes the pull up and pull down resistors form the GPIO inputs?