Other Parts Discussed in Thread: C2000WARE
Dear Expert ,
Good day!
Our customer want to confirm the details of the TMS320F28335 , in the TMS320x2833x, TMS320x2823x Technical Reference Manual chapter 12.12.1 McBSP Receive Interrupt Generation
There is the OR gate with 2 input :RINT and RINTENA , from the descriptions , the RINTENA looks like the enable trigger of the OR gate , but except this chapter , I can not find any other information about this signal , please help me to confirm the query below
1 . The RINTENA is the OR gate enable signal or it is one of the OR gate input .
2. Could it be configurated ?If yes , please tell me which register could configurate it ,if not , the default value is ?
The customer want to program the driver of this device , so they want to confirm the details of this interrupt .
BR,
Leon.liu