Part Number: DRV8301-69M-KIT
Hi TI,
We are using Direct drive motor which operates at 310DC and1.5A. Along with this motor we are using DRV8301-69M-KIT(operated at 55V) with 28069F MCU for identification of the motor parameters.
During Rs identification motor is running properly and Rs is identified but when the Lq/Ld identification motor struggles to rotate and identification are not proper.
How can we get the correct paraments of motor.
Thanks