Other Parts Discussed in Thread: MOTORWARE
I'm running into a strange issue while trying to debug an Instaspin motorware application on the F28069F. When I run the debugger in CCS the mainISR seems to be executing at a much slower rate than it should be. The mainISR should be triggered off the completion of the ADC interrupt but it seems to be at a much slower rate. I have one breakpoint that updates the expression view enable and its in the main function, not mainISR. Without the breakpoint enable I think it executes at the correct rate. Not sure as I can't debug it. Still issues with the code but can't see the expressions to debug. The other strange thing is if I setup the breakpoint to update all windows it doesn't update the expressions and the code doesn't seem to execute fully. It does turn on the status LED of my board but doesn't turn on the Run_Identify flag which turns on another LED. I think it may be halting execution instead of continuing.
This wasn't an issue until recently, so I'm sure I fat fingered something. What am I missing.
Thanks, John