Other Parts Discussed in Thread: UNIFLASH
Hello TI support team,
I'm working on the programming driver of TMS320F280048 via JTAG. Unfortunately I'm not able to write our application to LSx RAM blocks, but only to Mx RAM blocks (if I read the data back, I always see 0x00). Since we perform also a C28x Emulation reset, I'm not sure if we should are missing something during the initialization of the device. In fact, I see several actions in the GEL file made for Uniflash. For example, I see on page 142 of "SPRUI33D – NOVEMBER 2015 – REVISED SEPTEMBER 2020" that some dummy reads should be performed.
How should we disable the DCSM protection on LSx RAM blocks?
Do we have to call the BOOT ROM init code?
Thanks in advance for your support!