Other Parts Discussed in Thread: TMS320F280025C,
Hi,
I am working on a project using different MCUs(TMS320F28388D & TMS320F280025C).
I am trying to use a single JTAG for different MCUs, but I am wondering
if it is possible to configure the circuit as shown in the figure below.
In addition, the projects using CCS are as follows.
[Fig.1]
[Fig.2]
[Questions]
1. If the circuit is configured as shown in Figure 1, is it possible to connect to different MCUs with one JTAG?
2. If the project is configured as shown in Figure 2, is it possible to download programs to different MCUs with one JTAG?
Thank you.
Regard,
Lyoo