Hello. I am interested in using EPWM1 through EPWM16 on the 28388 processor. The TMDSCNCD2838x_RevB_180cCARD_pinout.pdf file shows that, for example, pin 67 is SPISIMO. However the schematic routes the signal to pin E1 of the BGA, which is GPIO_16, which can also be used (per the TMS320F2838x datasheet) for EPWM9A.
Is there anything about the controlCARD that will prevent using the GPIO pins as EPWM? See attachment below.
Best Regards, Charlie