Hi,
I am working on the CM core and when I defined a uint32_T variable it appears to generate a unsigned int variable. for example in the below code
when I ctrl=left click o nthe uint32_t it will point me to unsigned int - see below
first I select the right code generation tools
and than I end up at
which is unsigned int.
I also looked with the debugger - when I add the expressing to a watch window it becomes unsigned int.
can you explain why ? what am I missing ?